The voltage range of MicPhone signal is usually between 0~3.3V. Can ADS8568 accept this unipolar analog input signal?So, can HVDD connect to 3.3V and HVSS connect to Ground?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ray,
Thank you for your post and welcome to our forum!
The ADS8568 requires two pairs of analog supply voltages: AVDD / AVSS and HVDD / HVSS. The HVDD / HVSS supplies are intended to allow the analog inputs to accept single-ended, bipolar signals. If your input signal only ranges from 0 - 3.3 V, you may use HVDD = 3.3 V and HVSS = GND. Please refer to the Recommended Operating Conditions table for recommended supply configurations.
Regards,
Hello Ryan,
Thanks for your reply!
According to the Recommended Operating Conditions table: 5V < HVDD < 16.5V , -16.5V < HVSS< -5V. However, the Absolute Maximum Ratings table shows : -0.3V < HVDD < 18V , -18V < HVSS < -0.3V.
If, I still use HVDD = 3.3 V and HVSS = GND. What problems may be caused in this case?
Alternatively, can I use HVDD =5V and HVSS = -5V ?It covers the range of 0 - 3.3V
Hello Ray,
Reducing the HVDD/HVSS supply to only 3.3 V and 0 V may lead to degraded performance. Please follow the guidelines in table 7.3.
+/- 5 V for the HVDD/HVSS supplies is ok.
Regards,