Other Parts Discussed in Thread: ADS7945,
For SNR & SINAD performance @ 2 MSPS the data sheet lists performance only at 20 KHz input frequency. Are there plots for these out to Nyquist frequency (~1 MHz)? I would like to see how these parameters degrade as input frequency increases. Also, what is the input level for these measurements? If new data needs to be taken, please do it at full-scale input.