We designed the ADC circuit with ADS5270 to receive input voltage in the range of ±10V as follows.
And the output of the function generator and the value measured by ADS5270 were compared and tested with an oscilloscope through DAC.
As in the first picture, the measurement is well within the ±6V range, but beyond that range, noise is included as in the second picture.
We are wondering if there is a problem with the design of the input circuit composed of OP-AMPs.
Or is there a problem elsewhere?
Thanks a million,
Hyeong-Jin