Other Parts Discussed in Thread: REF5045
Hi Team,
I have a question on the use of an external reference voltage source for the ADS1605.
How do you solve the requirement of three different voltages (4V, 2,5V, and 1V) on the VREF pins of the ADC. There is also the problem that 4V and 1V is not really common as a voltage reference. Working with three separate voltage references will also reduce the available space on the PCB that could lead to a problem later on.
Is there an example or suggestion for using an external voltage reference with this ADC?
Thanks for your answer.
Best regards,
Thomas