This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38J84EVM: SerDes Linerate

Part Number: DAC38J84EVM
Other Parts Discussed in Thread: DAC38J82, LMK04832

HI Jim,

Is there any way I can force a different Linerate when the LMFS still the same? I am using LMFS=2221 and I would like to force the GUI to Linerate =3200 Mbps. The FPGA Clock , I would like to work with is 80MHz and the DAC Output Rate would be 1280MHz. The DAC Data Input Rate would be 284.44444MHZ.