This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ2700: Order of SYSREF auto calibration when device initialization

Part Number: ADC12DJ2700

Hello. 

I want to perform Automatic SYSREF Calibration, but I am wondering at what stage of the Initilization sequence should src_en be set to 1.

In other words, I am curious what normal operation condition means to start Automatic SYSREF Calibration.

---------------------------------------------------------------------------

8.3 Initialization Set Up

The device and JESD204 interface require a specific startup and alignment sequence. The general order of that sequence is listed in the following steps.

1. Power-up or reset the device.
2. Apply a stable device CLK signal at the desired frequency.
3. Program JESD_EN = 0 to stop the JESD204B state machine and allow setting changes.
4. Program CAL_EN = 0 to stop the calibration state machine and allow setting changes.
5. Program the desired JMODE.
6. Program the desired KM1 value. KM1 = K-1.
7. Program SYNC_SEL as needed. Choose SYNCSE or timestamp differential inputs.
8. Configure device calibration settings as desired. Select foreground or background calibration modes and offset calibration as needed.
9. Program CAL_EN = 1 to enable the calibration state machine.
10. Enable overrange via OVR_EN and adjust settings if desired.
11. Program JESD_EN = 1 to re-start the JESD204B state machine and allow the link to restart.
12. The JESD204B interface operates in response to the applied SYNC signal from the receiver.
13. Program CAL_SOFT_TRIG = 0.
14. Program CAL_SOFT_TRIG = 1 to initiate a calibration.

---------------------------------------------------------------------------

7.3.5.3.2

~The ADC12DJ2700 must have a proper device clock applied and be programmed for normal operation before

starting the automatic SYSREF calibration.