Other Parts Discussed in Thread: ADS1258
Hello team,
My customer is performing some testing with ADS1258-EP. They wanted to share these results and see any suggestion on how to improve accuracy from the ADC.
They are using the following configurations for this testing:
- Chopping is Enabled.
- Data Rate is set to 11
- Last 11 bits are masked off.
- Testing is done at ambient.
- Apply 1V precision input on AIN 11 of ADC, take 1000 samples, average them and read results.
- Apply 3V precision input on AIN 11 of ADC, take 1000 samples, average them and read results.
They are seeing the following results with this testing. There seems to be a lot of error in the results in un-calibrated section.
The customer has a few questions regarding these results below:
- Is there a way I can reduce the error in uncalibrated output? Because it is delta sigma converter so as per my understanding the results should be very good.
- The calibration (Straight Line Method) has been applied on only one of the chips to reduce offset and gain errors. Can we store these calibration coefficients in our micro controller memory and apply these coefficients to all the chips for different controllers?? Because offset and gain error will be different for different chips so I am not sure we can apply these calibration coefficients on other chips or not??
Thank you for your support!
Errol