Other Parts Discussed in Thread: ADS9224R
Greetings,
I have a question regarding the connection of NC pins on the THS4551IRUNR FD amplifier in the schematic of the evaluation board for the ADS9224R ADC. NC pin no. 2 is connected to the VA rail via 10k resistor, and NC pin no. 8 is connected to the REFP/2 (which is used for setting output common mode voltage) via RC filter.
Is there a reason for this since the datasheet for this amplifier doesn't mention where NC pins should be connected (it only notes that there is no internal connection)?
Can I leave NC pins floating, or connect them to other potential, for example GND?
Best regards,
Domagoj