Part Number: AMC1305M25
Hi,
When CLKIN=20MHz, is DOUT fixed to 10MHz since data change at CLKIN falling edge?
But how to understand the picture as below? when analog input increase, It seems not only the "1" density but also frequency changes.
customer test our AMC1305 with 0mV input. it shown as below:
the "1" density is 50%, no problem, but DOUT frequency is 10MHz or 5MHz. I assume that it's due to 01 01 01 01 or 01 10 01 10, its always 10MHz, but when it shown as 01 10 01 10, it looks like 5MHz. right? is it normal? thank you!
Best regards,
Yuan Tan