Hello everyone!
I am using ADS122C04 on a new project, and I have had problems with the PGA.
I put 3.3V voltage both digital and analog, both using the same GND.
I use an external 2.5V VREF. But I also tried using the internal VREF.
My problem is:
If I use the PGA with more than 4 (8, 16, 32 ...) the value that is converted is wrong, not linear.
A very small input signal, for example 150mV, if I set PGA = 4, the AD informs me 600mV. But if I put PGA = 8, I always see below, something like 975mV in the conversion.
What will it be? Is it a lack of bipolar voltage to excite the second stage of the PGA?
Thanks!