We are clocking this part at 150MHz with low latency mode and then sampling the CMOS output in an FPGA.
Sample clock is the ADS4126 input clock (i.e. not using CLKOUT).
I am trying to understand the time at which data will be valid relative to the rising edge of input clock.
Q1: In table 5 and taking 170MHz as example, is 1.5nS before the clock rising edge the EARLIEST or the LATEST time the data becomes valid?
We are extrapolating to 150MHz from the timing values in table 5 and using Tstart = -2.2nS and Tdv = 4.7/5.5.
Q2: Is this a valid approach?
Q3: If so, is rising edge-2.2 the earliest or the latest time that data becomes valid?
Thanks for any help.