I am designing a circuit using DA converter DAC5662.
Use the DAC5662 under the following conditions.
Use the DAC5662 under the following conditions.
- GSET pin : H level (+3.3V)
- DAC A ch : Use
- DAC B ch : Not use
Here, let's check if there is no problem with the following not used pin settings.
- IOUTB1 pin, IOUTB2 pin : not connect
- BIASJ_B pin : not connect
- DB11 pin to DB0 pin : connect GND
- CLKB pin : connect GND
- WRTB pin : connect GND
- BIASJ_B pin : not connect
- DB11 pin to DB0 pin : connect GND
- CLKB pin : connect GND
- WRTB pin : connect GND
Regards,
MESH