This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7718: Offset and power-on reset issue

Part Number: DAC7718

Hi,

There is wrong offset and abnormal output in power-on/off as below description.

1. OFFSET_A is around 2.6V at 000h with dual supply. When it's 800h, OFFSET_A was 0V.

2. Output is around -5V with RSTSEL->IOVDD, /USB/BTC ->IOVDD

Setting is

Configuration: 858h

Monitor: 000h

GPIO: E00h

Offset DAC-A: 000h

Offset DAC-B: 000h

SPI MODE: 000h

Read back is already done.

Output is 2.6V with 800h for 0V and 7.6V with 840h for 5V.

Schematic is as below.