Hi,
we would like to use an ADS1232 to convert the load cell of a weigh scale.
The load cell is supplied with 5V, has a nominal value of 2mV / V and therefore delivers a voltage of 10mV at full output (2,000kg).
Assuming the load cell is ideal -
What accuracy result are to be expected with the ADS1232? How many kg of deviation can be expected in the worst case?
In the data sheet of the ADS1232, tolerance ranges and maximum deviations are specified for some values and I am unsure how all these errors add up or whether I even consider all relevant parameters.
So it would be a great pleasure for me if you could perhaps offer me some support here.
Thank you in advance!
Alen