Other Parts Discussed in Thread: ADS1148
At present, I have a design idea to collect high voltage (100-800V) by means of resistance partial voltage;
I need the acquisition accuracy of the final system at 0.5%, each of the sample values, full temperature range(-40~85℃);
However, I am considering whether the 12-bit ADC can meet the requirements and whether there are relevant calculation methods for the true error of ADC;
At present, the errors I can identify come from the following aspects: ADC error, REF error, and the partial pressure resistance error;
Or is there any relevant calibration method for reference?
I think the price of a 12-bit ADC is cheap, therefore, should I obtain higher accuracy through calibration or choose a higher accuracy ADC(such as ADS1148)?
If you have good Suggestions, please help me choose;