Other Parts Discussed in Thread: TIDA-010037,
Hi Team,
A few question - looking at a split phase meter design with ANSI C12, 0.2 accuracy. Found the TIDA-010037 and the ADS131M04.
- would you recommend this device for the application?
- would this be capable of current control for the inverter with control BW of 4-10kHz?
- one of the issues with following the ref design is their DSP is in a different board so the SPI connects between boards with flat cables, but in this design it also takes the clock from the micro that is 8MHz, that will not work with flat cable. Would we be able to just replace it with a 8MHz oscillator, should that be ok? Will it cause any sync issue?
- can the ADS131M04 be used for general current sense as well for the inverter? It will be good if we can use the same current sensor for energy measurement and inverter current control.
- We are trying to figure out the BW of this ADC and BW after the SINC filter as the filter itself has a settling time of 1112clk for 2560SR
- can this IC be used without the filters as well?
I appreciate all the help you can provide!
Regards,
Ramon