Part Number: ADC32RF45EVM
Other Parts Discussed in Thread: LMK04828, ADC32RF45, LMX2582
We are using ADC32RFXX EVM GUI for configuring LMK04828 in our customized ADC32RF45 Board.We are getting proper clock input to LMK04828 from onboard crystal but DCLK clock is not coming out.We used DCLKOUT0 for the reference clock of FPGA.We are mounting FMC based ADC Board to our FPGA.Here are the details of clock and RF signal frequency for the setup.
1. ADC channel input is 200 MHz.
2. LMK04828 clock in is 122.8 MHz.
3. In ADC32RFXX EVM GUI- a) Clock source to ADC set as LMX2582 to ADC.
b) Internal clk Freq = 1536 Msps.
c) ADC32RF45 mode = DDC.
I need max 200 MHz FPGA reference clock from this ADC board. Can you please help me to configure PLL and other parameters of LMK04828 and LMX2582 to get this reference clock and ADC throughput.