Hello
I don`t understand ADC `s data output. I finded in the datasheet an explaination about it, but it didn`t clear for me.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I don`t understand ADC `s data output. I finded in the datasheet an explaination about it, but it didn`t clear for me.
Hi user6244799,
You ignore the LSB and only consider the MSB and mid-byte data. In your data the MSB = 0x00 and the mid-byte data is 0x32. The temperature sensor result is 14 bits left justified in the returned data, so 0x00 32 would be shifted right by two (>>2) which would leave a 14-bit result as 0x000C or decimal 12. 12 times the coefficient of 0.03125 deg C per code is 0.375 deg C.
I'm not sure if you have the part in an environment of that temperature, but that is the result from the data given. If you are expecting a room temperature value, then make sure that you have the TS bit set and also that you are reading the conversion data after setting the TS bit and the conversion has completed. The RDATA will read the last conversion completed and not necessarily the conversion after setting the TS bit.
Best regards,
Bob B
Thanks for your explain.
If I use no internal temperature sensor should I set TS bit on? As I understand it`s unneeded.
Hi user6244799,
To be more clear, when you want to use the internal temperature sensor you need to set the TS bit to 1. If you want to convert the analog inputs you need to set the TS bit to 0. You cannot measure both the internal temperature sensor and the analog inputs at the same time. It is just one or the other.
If the TS bit is 1 and the data retrieved is as you have shown, you totally ignore the LSB. You combine the MSB and mid-byte together and right shift by 2 (as the data is 14-bit left justified) to get a 14-bit result from the 16 bits of data.
(0000 1100 1110 0100b) >> 2 = (0000 0011 0011 1001b) = 339h = 825d
825 counts * 0.03125 deg C/count = 25.78 deg C
Best regards,
Bob B
If I use an external temperature sensor how receiving data should be converted? Like an internal one data?
Hi user6244799,
If you use an external temperature sensor such as a thermistor, thermocouple or RTD the measurement is much different between the sensors and is not at all calculated in the same way as the internal temperature sensor of the ADS122U04.
I would suggest reading the following:
A Basic Guide to Thermocouple Measurements
A Basic Guide to RTD Measurements
Best regards,
Bob B