Hi Team,
My customer use ADS7052IRUGR and found that it works abnormally when the temp is lower than -14℃.
Test environment: Thermometer box, which could keep temp to -25℃~0℃
Test method: Provide 2.048V DC signal to the input of ADS7052 and then read the value of ADC output through FPGA.
SCH:
Test Result:
Customer has confirmed that the input voltage(2.048V), the DVDD(3.3V) and AVDD(3.3V) are all normal during the temperature( -25℃~0℃).
However, when the temp is lower than -14℃, the output of the ADS7052 is abnormal. You could see that the result is only 600 and 0.311V...
Temp in temperate box/℃ | Actual input voltage/V | Read the result from ADC output | Calculated input voltage/V |
5 | 2.048 | 2742 | 2.024 |
0 | 2.048 | 2748 | 2.025 |
-5 | 2.048 | 274F | 2.027 |
-10 | 2.048 | 2751 | 2.027 |
-14 | 2.048 | 600 | 0.309 |
-18 | 2.048 | 606 | 0.311 |
-23 | 2.048 | 608 | 0.311 |
It seems that ADS7052 is abnormal. Could you please kindly give some advice about this?
Thanks!