January 23rd 2020 there was an Application Advisory released that depicted the possible occurrence of sparkle codes under certain input voltage conditions.There is a table in the Application Advisory with some empirically observed results. According to this table, a negative sparkle code is only observed at ~3/4 from the full scale, all other potential sparkle codes going in the positive direction. But as this table is based on empirical results, it is not clear if the direction of the sparkle codes can be considered as systematic. In particular, could negative sparkle codes potentially be observed at 1/16, 1/8, 1/4, 1/2 or 5/8 input levels?
Thank you.
David