Hi team,
On the question of AMC7812B. Currently our software uses direct mode, and now I want to switch to auto mode. But on the hardware, _DAV (pin 2) and _CNVT (pin 3) are not connected to the main control device.
We are worried that when switching to auto mode, these two signals are not connected, as shown in the following timing diagram
If the software reads the contents of the register when _DAV is high, it means that the ADC conversion has not been completed at the current moment. Is the value read at this time the stable value at the previous sampling time or an invalid value?