Hi,
I have the ADC with the following clocks:
Fclk (system clock) = 4.000 MHz
SCLK (SPI serial clock) = 2 MHz
I have a sampling rate of 976.6 s/s (equal to 1/1024).
How is possible to obtain exactly the data rate of 1ks/s?
Maybe I need to use an Fclsk of 4.096 MHz instead 4.000 MHz?
Are there any other actions to obtain a data rate of exactly 1ks/s?
The SCLK frequency influences in some way the data rate?
Thank you very much
Davide Badoni