Other Parts Discussed in Thread: ADS7951
Hi,
What is the unused pin recommendation for unused ADC input channels and unused GPIOs for ADS7951?
Also what to do with the NC pins(pin 15 and 16).Should it be grounded via zero ohm resistor?
Thanks,
Hima
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
What is the unused pin recommendation for unused ADC input channels and unused GPIOs for ADS7951?
Also what to do with the NC pins(pin 15 and 16).Should it be grounded via zero ohm resistor?
Thanks,
Hima
Hello Hima,
The analog input pins should be grounded. The unused GPIO can be left floating.
The NC are pins that have no internal connection. There can usually be left floating, but the datasheet states not to do so; thus to be safe I suggest to ground the NC pins
Regards
Cynthia