I have been testing with this device and I have come across a problem with the noise on the input of the ADC, which is about 0.270 mV. Also with the use of the voltage divider I get a weird offset and it is not working properly. The Input signal I use is with the function generator, which is a 50 Hz 20 mVpp signal.