This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF45: Unable to read Digital bank registers but able read Analog bank and direct addressees bank registers

Part Number: ADC32RF45

i amusing the adc32rf45 custom. ADC mode is 8224 and Fs is 2.5Ghz. 

when i configurating the adc i am unable read Digital bank Registers. but i am able read analog bank registers.

  • Hi Bala Krishna,

    Are you using 3-wire or 4 wire SPI mode? When using 3-wire SPI, digital register bank read back doesn't work. You can use 4-wire mode for digital bank read-back.

    We are yet to update this in the datasheet. 

    Regards,

    Vijay

  • Hi Vijay, 

    we are using 4-wire spi mode only.but still we are not to read digital bank registers.

    Regards

    Bala Krishna 

  • Hi Bala Krishna,

    After hardware reset, before Digital bank can be programmed, analog powerup config has to be run. This config is in Powerup_Analog_Config.cfg in Configuration files. (Configuration files are available at: https://www.ti.com/lit/zip/sbaa226

    I verified on ADC32RF45EVM that SPI read is working for all digital banks (Offset correction, Digital Gain and JESD) after analog powerup config is ran. 4 wire SPI is used on the EVM. Please check digital bank read after running Powerup_Analog_Config.cfg.

    Regards,

    Vijay

  • Hi Vijay,

    we are following the same procedure but still we are unable to read digital bank registers.we are using LMFS=8224 Bypass Mode. Please send the configuration files for 8224 bypass mode.

    Regards

    Bala Krishna

  • Hi vijay,

    with the above given configuration, we are able to read only some digital but not all registers. with the given configuration we are still getting JESD lane errors. Please provide configuration file for Bypass mode 8224 mode not for DDC mode.

    Thanks & Regards,

    Bala Krishna  

  • Hi Bala Krishna,

    The config I sent is for bypass mode with LMFS: 8224. I have verified it on TI EVM. JESD K is set to 16 and LVDS SYNC is used. Are you using the same? Is SYSREF to ADC turned on during configuration? What is the SYSREF frequency being used?

    I verified that read is working from offset correction, Digital Gain and JESD pages. can you please tell which digital pages you are able to read back and which pages aren't working? Can you please double check the page selection writes. It is unlikely that some digital banks are working while other are not. 

    Regards,

    Vijay

  • Hi Vijay,

    we are unable write/read JESD Page registers and other page registers are also not read properly.Please find the attached register log of ADC.

    Thanks & Regards

    Bala Krishna

    ADC_Reg_log.txt
    /*********************************No of Register Written Count: 0**********************************/
    SPI ADC Write (24-bit)  value:0x81
    SPI ADC Read  (24-bit)  value:0x800081
    SPI ADC Read Byte value:0x3C
    /*********************************No of Register Written Count: 1**********************************/
    SPI ADC Write (24-bit)  value:0x11FF
    SPI ADC Read  (24-bit)  value:0x8011FF
    SPI ADC Read Byte value:0xFF
    /*********************************No of Register Written Count: 2**********************************/
    SPI ADC Write (24-bit)  value:0x22C0
    SPI ADC Read  (24-bit)  value:0x8022C0
    SPI ADC Read Byte value:0xC0
    /*********************************No of Register Written Count: 3**********************************/
    SPI ADC Write (24-bit)  value:0x3280
    SPI ADC Read  (24-bit)  value:0x803280
    SPI ADC Read Byte value:0x80
    /*********************************No of Register Written Count: 4**********************************/
    SPI ADC Write (24-bit)  value:0x3308
    SPI ADC Read  (24-bit)  value:0x803308
    SPI ADC Read Byte value:0x8
    /*********************************No of Register Written Count: 5**********************************/
    SPI ADC Write (24-bit)  value:0x4203
    SPI ADC Read  (24-bit)  value:0x804203
    SPI ADC Read Byte value:0x3
    /*********************************No of Register Written Count: 6**********************************/
    SPI ADC Write (24-bit)  value:0x4303
    SPI ADC Read  (24-bit)  value:0x804303
    SPI ADC Read Byte value:0x3
    /*********************************No of Register Written Count: 7**********************************/
    SPI ADC Write (24-bit)  value:0x4558
    SPI ADC Read  (24-bit)  value:0x804558
    SPI ADC Read Byte value:0x58
    /*********************************No of Register Written Count: 8**********************************/
    SPI ADC Write (24-bit)  value:0x46C4
    SPI ADC Read  (24-bit)  value:0x8046C4
    SPI ADC Read Byte value:0xC4
    /*********************************No of Register Written Count: 9**********************************/
    SPI ADC Write (24-bit)  value:0x4701
    SPI ADC Read  (24-bit)  value:0x804701
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 10**********************************/
    SPI ADC Write (24-bit)  value:0x5301
    SPI ADC Read  (24-bit)  value:0x805301
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 11**********************************/
    SPI ADC Write (24-bit)  value:0x5408
    SPI ADC Read  (24-bit)  value:0x805408
    SPI ADC Read Byte value:0x8
    /*********************************No of Register Written Count: 12**********************************/
    SPI ADC Write (24-bit)  value:0x6405
    SPI ADC Read  (24-bit)  value:0x806405
    SPI ADC Read Byte value:0x5
    /*********************************No of Register Written Count: 13**********************************/
    SPI ADC Write (24-bit)  value:0x7284
    SPI ADC Read  (24-bit)  value:0x807284
    SPI ADC Read Byte value:0x84
    /*********************************No of Register Written Count: 14**********************************/
    SPI ADC Write (24-bit)  value:0x8C80
    SPI ADC Read  (24-bit)  value:0x808C80
    SPI ADC Read Byte value:0x80
    /*********************************No of Register Written Count: 15**********************************/
    SPI ADC Write (24-bit)  value:0x9780
    SPI ADC Read  (24-bit)  value:0x809780
    SPI ADC Read Byte value:0x80
    /*********************************No of Register Written Count: 16**********************************/
    SPI ADC Write (24-bit)  value:0xF038
    SPI ADC Read  (24-bit)  value:0x80F038
    SPI ADC Read Byte value:0x38
    /*********************************No of Register Written Count: 17**********************************/
    SPI ADC Write (24-bit)  value:0xF1BF
    SPI ADC Read  (24-bit)  value:0x80F1BF
    SPI ADC Read Byte value:0xBF
    /*********************************No of Register Written Count: 18**********************************/
    SPI ADC Write (24-bit)  value:0x1100
    SPI ADC Read  (24-bit)  value:0x801100
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 19**********************************/
    SPI ADC Write (24-bit)  value:0x1204
    SPI ADC Read  (24-bit)  value:0x801204
    SPI ADC Read Byte value:0x4
    /*********************************No of Register Written Count: 20**********************************/
    SPI ADC Write (24-bit)  value:0x2501
    SPI ADC Read  (24-bit)  value:0x802501
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 21**********************************/
    SPI ADC Write (24-bit)  value:0x2640
    SPI ADC Read  (24-bit)  value:0x802640
    SPI ADC Read Byte value:0x40
    /*********************************No of Register Written Count: 22**********************************/
    SPI ADC Write (24-bit)  value:0x2780
    SPI ADC Read  (24-bit)  value:0x802780
    SPI ADC Read Byte value:0x80
    /*********************************No of Register Written Count: 23**********************************/
    SPI ADC Write (24-bit)  value:0x2940
    SPI ADC Read  (24-bit)  value:0x802940
    SPI ADC Read Byte value:0x40
    /*********************************No of Register Written Count: 24**********************************/
    SPI ADC Write (24-bit)  value:0x2A80
    SPI ADC Read  (24-bit)  value:0x802A80
    SPI ADC Read Byte value:0x80
    /*********************************No of Register Written Count: 25**********************************/
    SPI ADC Write (24-bit)  value:0x2C40
    SPI ADC Read  (24-bit)  value:0x802C40
    SPI ADC Read Byte value:0x40
    /*********************************No of Register Written Count: 26**********************************/
    SPI ADC Write (24-bit)  value:0x2D80
    SPI ADC Read  (24-bit)  value:0x802D80
    SPI ADC Read Byte value:0x80
    /*********************************No of Register Written Count: 27**********************************/
    SPI ADC Write (24-bit)  value:0x2F40
    SPI ADC Read  (24-bit)  value:0x802F40
    SPI ADC Read Byte value:0x40
    /*********************************No of Register Written Count: 28**********************************/
    SPI ADC Write (24-bit)  value:0x3401
    SPI ADC Read  (24-bit)  value:0x803401
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 29**********************************/
    SPI ADC Write (24-bit)  value:0x3F01
    SPI ADC Read  (24-bit)  value:0x803F01
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 30**********************************/
    SPI ADC Write (24-bit)  value:0x3950
    SPI ADC Read  (24-bit)  value:0x803950
    SPI ADC Read Byte value:0x50
    /*********************************No of Register Written Count: 31**********************************/
    SPI ADC Write (24-bit)  value:0x3B28
    SPI ADC Read  (24-bit)  value:0x803B28
    SPI ADC Read Byte value:0x28
    /*********************************No of Register Written Count: 32**********************************/
    SPI ADC Write (24-bit)  value:0x4080
    SPI ADC Read  (24-bit)  value:0x804080
    SPI ADC Read Byte value:0x80
    /*********************************No of Register Written Count: 33**********************************/
    SPI ADC Write (24-bit)  value:0x4240
    SPI ADC Read  (24-bit)  value:0x804240
    SPI ADC Read Byte value:0x40
    /*********************************No of Register Written Count: 34**********************************/
    SPI ADC Write (24-bit)  value:0x4380
    SPI ADC Read  (24-bit)  value:0x804380
    SPI ADC Read Byte value:0x80
    /*********************************No of Register Written Count: 35**********************************/
    SPI ADC Write (24-bit)  value:0x4540
    SPI ADC Read  (24-bit)  value:0x804540
    SPI ADC Read Byte value:0x40
    /*********************************No of Register Written Count: 36**********************************/
    SPI ADC Write (24-bit)  value:0x4680
    SPI ADC Read  (24-bit)  value:0x804680
    SPI ADC Read Byte value:0x80
    /*********************************No of Register Written Count: 37**********************************/
    SPI ADC Write (24-bit)  value:0x4840
    SPI ADC Read  (24-bit)  value:0x804840
    SPI ADC Read Byte value:0x40
    /*********************************No of Register Written Count: 38**********************************/
    SPI ADC Write (24-bit)  value:0x4980
    SPI ADC Read  (24-bit)  value:0x804980
    SPI ADC Read Byte value:0x80
    /*********************************No of Register Written Count: 39**********************************/
    SPI ADC Write (24-bit)  value:0x4B40
    SPI ADC Read  (24-bit)  value:0x804B40
    SPI ADC Read Byte value:0x40
    /*********************************No of Register Written Count: 40**********************************/
    SPI ADC Write (24-bit)  value:0x5360
    SPI ADC Read  (24-bit)  value:0x805360
    SPI ADC Read Byte value:0x60
    /*********************************No of Register Written Count: 41**********************************/
    SPI ADC Write (24-bit)  value:0x5902
    SPI ADC Read  (24-bit)  value:0x805902
    SPI ADC Read Byte value:0x2
    /*********************************No of Register Written Count: 42**********************************/
    SPI ADC Write (24-bit)  value:0x5B08
    SPI ADC Read  (24-bit)  value:0x805B08
    SPI ADC Read Byte value:0x8
    /*********************************No of Register Written Count: 43**********************************/
    SPI ADC Write (24-bit)  value:0x5C07
    SPI ADC Read  (24-bit)  value:0x805C07
    SPI ADC Read Byte value:0x7
    /*********************************No of Register Written Count: 44**********************************/
    SPI ADC Write (24-bit)  value:0x5710
    SPI ADC Read  (24-bit)  value:0x805710
    SPI ADC Read Byte value:0x10
    /*********************************No of Register Written Count: 45**********************************/
    SPI ADC Write (24-bit)  value:0x5718
    SPI ADC Read  (24-bit)  value:0x805718
    SPI ADC Read Byte value:0x18
    /*********************************No of Register Written Count: 46**********************************/
    SPI ADC Write (24-bit)  value:0x5710
    SPI ADC Read  (24-bit)  value:0x805710
    SPI ADC Read Byte value:0x10
    /*********************************No of Register Written Count: 47**********************************/
    SPI ADC Write (24-bit)  value:0x5718
    SPI ADC Read  (24-bit)  value:0x805718
    SPI ADC Read Byte value:0x18
    /*********************************No of Register Written Count: 48**********************************/
    SPI ADC Write (24-bit)  value:0x5710
    SPI ADC Read  (24-bit)  value:0x805710
    SPI ADC Read Byte value:0x10
    /*********************************No of Register Written Count: 49**********************************/
    SPI ADC Write (24-bit)  value:0x5700
    SPI ADC Read  (24-bit)  value:0x805700
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 50**********************************/
    SPI ADC Write (24-bit)  value:0x1200
    SPI ADC Read  (24-bit)  value:0x801200
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 51**********************************/
    SPI ADC Write (24-bit)  value:0x11FF
    SPI ADC Read  (24-bit)  value:0x8011FF
    SPI ADC Read Byte value:0xFF
    /*********************************No of Register Written Count: 52**********************************/
    SPI ADC Write (24-bit)  value:0x8307
    SPI ADC Read  (24-bit)  value:0x808307
    SPI ADC Read Byte value:0x7
    /*********************************No of Register Written Count: 53**********************************/
    SPI ADC Write (24-bit)  value:0x5C00
    SPI ADC Read  (24-bit)  value:0x805C00
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 54**********************************/
    SPI ADC Write (24-bit)  value:0x5C01
    SPI ADC Read  (24-bit)  value:0x805C01
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 55**********************************/
    SPI ADC Write (24-bit)  value:0x1100
    SPI ADC Read  (24-bit)  value:0x801100
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 56**********************************/
    SPI ADC Write (24-bit)  value:0x400100
    SPI ADC Read  (24-bit)  value:0xC00100
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 57**********************************/
    SPI ADC Write (24-bit)  value:0x400200
    SPI ADC Read  (24-bit)  value:0xC00200
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 58**********************************/
    SPI ADC Write (24-bit)  value:0x400300
    SPI ADC Read  (24-bit)  value:0xC00300
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 59**********************************/
    SPI ADC Write (24-bit)  value:0x400461
    SPI ADC Read  (24-bit)  value:0xC00461
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 60**********************************/
    SPI ADC Write (24-bit)  value:0x606842
    SPI ADC Read  (24-bit)  value:0xE06842
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 61**********************************/
    SPI ADC Write (24-bit)  value:0x400301
    SPI ADC Read  (24-bit)  value:0xC00301
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 62**********************************/
    SPI ADC Write (24-bit)  value:0x606842
    SPI ADC Read  (24-bit)  value:0xE06842
    SPI ADC Read Byte value:0x42
    /*********************************No of Register Written Count: 63**********************************/
    SPI ADC Write (24-bit)  value:0x400100
    SPI ADC Read  (24-bit)  value:0xC00100
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 64**********************************/
    SPI ADC Write (24-bit)  value:0x400200
    SPI ADC Read  (24-bit)  value:0xC00200
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 65**********************************/
    SPI ADC Write (24-bit)  value:0x400300
    SPI ADC Read  (24-bit)  value:0xC00300
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 66**********************************/
    SPI ADC Write (24-bit)  value:0x400468
    SPI ADC Read  (24-bit)  value:0xC00468
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 67**********************************/
    SPI ADC Write (24-bit)  value:0x604401
    SPI ADC Read  (24-bit)  value:0xE04401
    SPI ADC Read Byte value:0x42
    /*********************************No of Register Written Count: 68**********************************/
    SPI ADC Write (24-bit)  value:0x606804
    SPI ADC Read  (24-bit)  value:0xE06804
    SPI ADC Read Byte value:0x42
    /*********************************No of Register Written Count: 69**********************************/
    SPI ADC Write (24-bit)  value:0x60FFC0
    SPI ADC Read  (24-bit)  value:0xE0FFC0
    SPI ADC Read Byte value:0x4
    /*********************************No of Register Written Count: 70**********************************/
    SPI ADC Write (24-bit)  value:0x60A208
    SPI ADC Read  (24-bit)  value:0xE0A208
    SPI ADC Read Byte value:0x4
    /*********************************No of Register Written Count: 71**********************************/
    SPI ADC Write (24-bit)  value:0x60A903
    SPI ADC Read  (24-bit)  value:0xE0A903
    SPI ADC Read Byte value:0x8
    /*********************************No of Register Written Count: 72**********************************/
    SPI ADC Write (24-bit)  value:0x60AB77
    SPI ADC Read  (24-bit)  value:0xE0AB77
    SPI ADC Read Byte value:0x3
    /*********************************No of Register Written Count: 73**********************************/
    SPI ADC Write (24-bit)  value:0x60AC01
    SPI ADC Read  (24-bit)  value:0xE0AC01
    SPI ADC Read Byte value:0x3
    /*********************************No of Register Written Count: 74**********************************/
    SPI ADC Write (24-bit)  value:0x60AD77
    SPI ADC Read  (24-bit)  value:0xE0AD77
    SPI ADC Read Byte value:0x3
    /*********************************No of Register Written Count: 75**********************************/
    SPI ADC Write (24-bit)  value:0x60AE01
    SPI ADC Read  (24-bit)  value:0xE0AE01
    SPI ADC Read Byte value:0x3
    /*********************************No of Register Written Count: 76**********************************/
    SPI ADC Write (24-bit)  value:0x60960F
    SPI ADC Read  (24-bit)  value:0xE0960F
    SPI ADC Read Byte value:0x3
    /*********************************No of Register Written Count: 77**********************************/
    SPI ADC Write (24-bit)  value:0x609726
    SPI ADC Read  (24-bit)  value:0xE09726
    SPI ADC Read Byte value:0x3
    /*********************************No of Register Written Count: 78**********************************/
    SPI ADC Write (24-bit)  value:0x608F0C
    SPI ADC Read  (24-bit)  value:0xE08F0C
    SPI ADC Read Byte value:0x26
    /*********************************No of Register Written Count: 79**********************************/
    SPI ADC Write (24-bit)  value:0x608C08
    SPI ADC Read  (24-bit)  value:0xE08C08
    SPI ADC Read Byte value:0xC
    /*********************************No of Register Written Count: 80**********************************/
    SPI ADC Write (24-bit)  value:0x60800F
    SPI ADC Read  (24-bit)  value:0xE0800F
    SPI ADC Read Byte value:0x8
    /*********************************No of Register Written Count: 81**********************************/
    SPI ADC Write (24-bit)  value:0x6081CB
    SPI ADC Read  (24-bit)  value:0xE081CB
    SPI ADC Read Byte value:0xF
    /*********************************No of Register Written Count: 82**********************************/
    SPI ADC Write (24-bit)  value:0x607D03
    SPI ADC Read  (24-bit)  value:0xE07D03
    SPI ADC Read Byte value:0xF
    /*********************************No of Register Written Count: 83**********************************/
    SPI ADC Write (24-bit)  value:0x605675
    SPI ADC Read  (24-bit)  value:0xE05675
    SPI ADC Read Byte value:0x3
    /*********************************No of Register Written Count: 84**********************************/
    SPI ADC Write (24-bit)  value:0x605775
    SPI ADC Read  (24-bit)  value:0xE05775
    SPI ADC Read Byte value:0x75
    /*********************************No of Register Written Count: 85**********************************/
    SPI ADC Write (24-bit)  value:0x605300
    SPI ADC Read  (24-bit)  value:0xE05300
    SPI ADC Read Byte value:0x75
    /*********************************No of Register Written Count: 86**********************************/
    SPI ADC Write (24-bit)  value:0x604B03
    SPI ADC Read  (24-bit)  value:0xE04B03
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 87**********************************/
    SPI ADC Write (24-bit)  value:0x604980
    SPI ADC Read  (24-bit)  value:0xE04980
    SPI ADC Read Byte value:0x3
    /*********************************No of Register Written Count: 88**********************************/
    SPI ADC Write (24-bit)  value:0x604326
    SPI ADC Read  (24-bit)  value:0xE04326
    SPI ADC Read Byte value:0x3
    /*********************************No of Register Written Count: 89**********************************/
    SPI ADC Write (24-bit)  value:0x605E01
    SPI ADC Read  (24-bit)  value:0xE05E01
    SPI ADC Read Byte value:0x26
    /*********************************No of Register Written Count: 90**********************************/
    SPI ADC Write (24-bit)  value:0x604238
    SPI ADC Read  (24-bit)  value:0xE04238
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 91**********************************/
    SPI ADC Write (24-bit)  value:0x605A04
    SPI ADC Read  (24-bit)  value:0xE05A04
    SPI ADC Read Byte value:0x38
    /*********************************No of Register Written Count: 92**********************************/
    SPI ADC Write (24-bit)  value:0x607120
    SPI ADC Read  (24-bit)  value:0xE07120
    SPI ADC Read Byte value:0x4
    /*********************************No of Register Written Count: 93**********************************/
    SPI ADC Write (24-bit)  value:0x606200
    SPI ADC Read  (24-bit)  value:0xE06200
    SPI ADC Read Byte value:0x20
    /*********************************No of Register Written Count: 94**********************************/
    SPI ADC Write (24-bit)  value:0x609800
    SPI ADC Read  (24-bit)  value:0xE09800
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 95**********************************/
    SPI ADC Write (24-bit)  value:0x609908
    SPI ADC Read  (24-bit)  value:0xE09908
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 96**********************************/
    SPI ADC Write (24-bit)  value:0x609C08
    SPI ADC Read  (24-bit)  value:0xE09C08
    SPI ADC Read Byte value:0x8
    /*********************************No of Register Written Count: 97**********************************/
    SPI ADC Write (24-bit)  value:0x609D20
    SPI ADC Read  (24-bit)  value:0xE09D20
    SPI ADC Read Byte value:0x8
    /*********************************No of Register Written Count: 98**********************************/
    SPI ADC Write (24-bit)  value:0x60BE03
    SPI ADC Read  (24-bit)  value:0xE0BE03
    SPI ADC Read Byte value:0x20
    /*********************************No of Register Written Count: 99**********************************/
    SPI ADC Write (24-bit)  value:0x606900
    SPI ADC Read  (24-bit)  value:0xE06900
    SPI ADC Read Byte value:0x20
    /*********************************No of Register Written Count: 100**********************************/
    SPI ADC Write (24-bit)  value:0x604510
    SPI ADC Read  (24-bit)  value:0xE04510
    SPI ADC Read Byte value:0x20
    /*********************************No of Register Written Count: 101**********************************/
    SPI ADC Write (24-bit)  value:0x608D64
    SPI ADC Read  (24-bit)  value:0xE08D64
    SPI ADC Read Byte value:0x10
    /*********************************No of Register Written Count: 102**********************************/
    SPI ADC Write (24-bit)  value:0x608B20
    SPI ADC Read  (24-bit)  value:0xE08B20
    SPI ADC Read Byte value:0x10
    /*********************************No of Register Written Count: 103**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x10
    /*********************************No of Register Written Count: 104**********************************/
    SPI ADC Write (24-bit)  value:0x600001
    SPI ADC Read  (24-bit)  value:0xE00001
    SPI ADC Read Byte value:0x10
    /*********************************No of Register Written Count: 105**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x10
    /*********************************No of Register Written Count: 106**********************************/
    SPI ADC Write (24-bit)  value:0x400100
    SPI ADC Read  (24-bit)  value:0xC00100
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 107**********************************/
    SPI ADC Write (24-bit)  value:0x400200
    SPI ADC Read  (24-bit)  value:0xC00200
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 108**********************************/
    SPI ADC Write (24-bit)  value:0x400301
    SPI ADC Read  (24-bit)  value:0xC00301
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 109**********************************/
    SPI ADC Write (24-bit)  value:0x400468
    SPI ADC Read  (24-bit)  value:0xC00468
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 110**********************************/
    SPI ADC Write (24-bit)  value:0x604980
    SPI ADC Read  (24-bit)  value:0xE04980
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 111**********************************/
    SPI ADC Write (24-bit)  value:0x604220
    SPI ADC Read  (24-bit)  value:0xE04220
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 112**********************************/
    SPI ADC Write (24-bit)  value:0x60A208
    SPI ADC Read  (24-bit)  value:0xE0A208
    SPI ADC Read Byte value:0x20
    /*********************************No of Register Written Count: 113**********************************/
    SPI ADC Write (24-bit)  value:0x400300
    SPI ADC Read  (24-bit)  value:0xC00300
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 114**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x20
    /*********************************No of Register Written Count: 115**********************************/
    SPI ADC Write (24-bit)  value:0x600001
    SPI ADC Read  (24-bit)  value:0xE00001
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 116**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 117**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 118**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 119**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 120**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 121**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 122**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 123**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 124**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 125**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 126**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 127**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 128**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 129**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 130**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 131**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 132**********************************/
    SPI ADC Write (24-bit)  value:0x600000
    SPI ADC Read  (24-bit)  value:0xE00000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 133**********************************/
    SPI ADC Write (24-bit)  value:0x400300
    SPI ADC Read  (24-bit)  value:0xC00300
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 134**********************************/
    SPI ADC Write (24-bit)  value:0x400420
    SPI ADC Read  (24-bit)  value:0xC00420
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 135**********************************/
    SPI ADC Write (24-bit)  value:0x4002F8
    SPI ADC Read  (24-bit)  value:0xC002F8
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 136**********************************/
    SPI ADC Write (24-bit)  value:0x603CF5
    SPI ADC Read  (24-bit)  value:0xE03CF5
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 137**********************************/
    SPI ADC Write (24-bit)  value:0x603D01
    SPI ADC Read  (24-bit)  value:0xE03D01
    SPI ADC Read Byte value:0xF5
    /*********************************No of Register Written Count: 138**********************************/
    SPI ADC Write (24-bit)  value:0x603EF0
    SPI ADC Read  (24-bit)  value:0xE03EF0
    SPI ADC Read Byte value:0xF5
    /*********************************No of Register Written Count: 139**********************************/
    SPI ADC Write (24-bit)  value:0x603F0C
    SPI ADC Read  (24-bit)  value:0xE03F0C
    SPI ADC Read Byte value:0xF0
    /*********************************No of Register Written Count: 140**********************************/
    SPI ADC Write (24-bit)  value:0x60400A
    SPI ADC Read  (24-bit)  value:0xE0400A
    SPI ADC Read Byte value:0xF0
    /*********************************No of Register Written Count: 141**********************************/
    SPI ADC Write (24-bit)  value:0x6041FE
    SPI ADC Read  (24-bit)  value:0xE041FE
    SPI ADC Read Byte value:0xA
    /*********************************No of Register Written Count: 142**********************************/
    SPI ADC Write (24-bit)  value:0x6053F5
    SPI ADC Read  (24-bit)  value:0xE053F5
    SPI ADC Read Byte value:0xA
    /*********************************No of Register Written Count: 143**********************************/
    SPI ADC Write (24-bit)  value:0x605401
    SPI ADC Read  (24-bit)  value:0xE05401
    SPI ADC Read Byte value:0xF5
    /*********************************No of Register Written Count: 144**********************************/
    SPI ADC Write (24-bit)  value:0x6055EE
    SPI ADC Read  (24-bit)  value:0xE055EE
    SPI ADC Read Byte value:0xF5
    /*********************************No of Register Written Count: 145**********************************/
    SPI ADC Write (24-bit)  value:0x60560E
    SPI ADC Read  (24-bit)  value:0xE0560E
    SPI ADC Read Byte value:0xF5
    /*********************************No of Register Written Count: 146**********************************/
    SPI ADC Write (24-bit)  value:0x60570B
    SPI ADC Read  (24-bit)  value:0xE0570B
    SPI ADC Read Byte value:0xE
    /*********************************No of Register Written Count: 147**********************************/
    SPI ADC Write (24-bit)  value:0x6058FE
    SPI ADC Read  (24-bit)  value:0xE058FE
    SPI ADC Read Byte value:0xB
    /*********************************No of Register Written Count: 148**********************************/
    SPI ADC Write (24-bit)  value:0x606AF4
    SPI ADC Read  (24-bit)  value:0xE06AF4
    SPI ADC Read Byte value:0xB
    /*********************************No of Register Written Count: 149**********************************/
    SPI ADC Write (24-bit)  value:0x606B01
    SPI ADC Read  (24-bit)  value:0xE06B01
    SPI ADC Read Byte value:0xB
    /*********************************No of Register Written Count: 150**********************************/
    SPI ADC Write (24-bit)  value:0x606CF0
    SPI ADC Read  (24-bit)  value:0xE06CF0
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 151**********************************/
    SPI ADC Write (24-bit)  value:0x606D0B
    SPI ADC Read  (24-bit)  value:0xE06D0B
    SPI ADC Read Byte value:0xF0
    /*********************************No of Register Written Count: 152**********************************/
    SPI ADC Write (24-bit)  value:0x606E09
    SPI ADC Read  (24-bit)  value:0xE06E09
    SPI ADC Read Byte value:0xF0
    /*********************************No of Register Written Count: 153**********************************/
    SPI ADC Write (24-bit)  value:0x606FFE
    SPI ADC Read  (24-bit)  value:0xE06FFE
    SPI ADC Read Byte value:0x9
    /*********************************No of Register Written Count: 154**********************************/
    SPI ADC Write (24-bit)  value:0x6081F5
    SPI ADC Read  (24-bit)  value:0xE081F5
    SPI ADC Read Byte value:0xFE
    /*********************************No of Register Written Count: 155**********************************/
    SPI ADC Write (24-bit)  value:0x608201
    SPI ADC Read  (24-bit)  value:0xE08201
    SPI ADC Read Byte value:0xFE
    /*********************************No of Register Written Count: 156**********************************/
    SPI ADC Write (24-bit)  value:0x6083EE
    SPI ADC Read  (24-bit)  value:0xE083EE
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 157**********************************/
    SPI ADC Write (24-bit)  value:0x60840D
    SPI ADC Read  (24-bit)  value:0xE0840D
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 158**********************************/
    SPI ADC Write (24-bit)  value:0x60850A
    SPI ADC Read  (24-bit)  value:0xE0850A
    SPI ADC Read Byte value:0xD
    /*********************************No of Register Written Count: 159**********************************/
    SPI ADC Write (24-bit)  value:0x6086FE
    SPI ADC Read  (24-bit)  value:0xE086FE
    SPI ADC Read Byte value:0xD
    /*********************************No of Register Written Count: 160**********************************/
    SPI ADC Write (24-bit)  value:0x6098FD
    SPI ADC Read  (24-bit)  value:0xE098FD
    SPI ADC Read Byte value:0xD
    /*********************************No of Register Written Count: 161**********************************/
    SPI ADC Write (24-bit)  value:0x609900
    SPI ADC Read  (24-bit)  value:0xE09900
    SPI ADC Read Byte value:0xFD
    /*********************************No of Register Written Count: 162**********************************/
    SPI ADC Write (24-bit)  value:0x609A00
    SPI ADC Read  (24-bit)  value:0xE09A00
    SPI ADC Read Byte value:0xFD
    /*********************************No of Register Written Count: 163**********************************/
    SPI ADC Write (24-bit)  value:0x609B00
    SPI ADC Read  (24-bit)  value:0xE09B00
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 164**********************************/
    SPI ADC Write (24-bit)  value:0x609C00
    SPI ADC Read  (24-bit)  value:0xE09C00
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 165**********************************/
    SPI ADC Write (24-bit)  value:0x609D00
    SPI ADC Read  (24-bit)  value:0xE09D00
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 166**********************************/
    SPI ADC Write (24-bit)  value:0x60AFFF
    SPI ADC Read  (24-bit)  value:0xE0AFFF
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 167**********************************/
    SPI ADC Write (24-bit)  value:0x60B000
    SPI ADC Read  (24-bit)  value:0xE0B000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 168**********************************/
    SPI ADC Write (24-bit)  value:0x60B101
    SPI ADC Read  (24-bit)  value:0xE0B101
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 169**********************************/
    SPI ADC Write (24-bit)  value:0x60B2FF
    SPI ADC Read  (24-bit)  value:0xE0B2FF
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 170**********************************/
    SPI ADC Write (24-bit)  value:0x60B3FF
    SPI ADC Read  (24-bit)  value:0xE0B3FF
    SPI ADC Read Byte value:0xFF
    /*********************************No of Register Written Count: 171**********************************/
    SPI ADC Write (24-bit)  value:0x60B400
    SPI ADC Read  (24-bit)  value:0xE0B400
    SPI ADC Read Byte value:0xFF
    /*********************************No of Register Written Count: 172**********************************/
    SPI ADC Write (24-bit)  value:0x60C6FE
    SPI ADC Read  (24-bit)  value:0xE0C6FE
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 173**********************************/
    SPI ADC Write (24-bit)  value:0x60C700
    SPI ADC Read  (24-bit)  value:0xE0C700
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 174**********************************/
    SPI ADC Write (24-bit)  value:0x60C800
    SPI ADC Read  (24-bit)  value:0xE0C800
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 175**********************************/
    SPI ADC Write (24-bit)  value:0x60C902
    SPI ADC Read  (24-bit)  value:0xE0C902
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 176**********************************/
    SPI ADC Write (24-bit)  value:0x60CA00
    SPI ADC Read  (24-bit)  value:0xE0CA00
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 177**********************************/
    SPI ADC Write (24-bit)  value:0x60CB00
    SPI ADC Read  (24-bit)  value:0xE0CB00
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 178**********************************/
    SPI ADC Write (24-bit)  value:0x60DDFF
    SPI ADC Read  (24-bit)  value:0xE0DDFF
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 179**********************************/
    SPI ADC Write (24-bit)  value:0x60DE00
    SPI ADC Read  (24-bit)  value:0xE0DE00
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 180**********************************/
    SPI ADC Write (24-bit)  value:0x60DF02
    SPI ADC Read  (24-bit)  value:0xE0DF02
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 181**********************************/
    SPI ADC Write (24-bit)  value:0x60E000
    SPI ADC Read  (24-bit)  value:0xE0E000
    SPI ADC Read Byte value:0x2
    /*********************************No of Register Written Count: 182**********************************/
    SPI ADC Write (24-bit)  value:0x60E1FE
    SPI ADC Read  (24-bit)  value:0xE0E1FE
    SPI ADC Read Byte value:0x2
    /*********************************No of Register Written Count: 183**********************************/
    SPI ADC Write (24-bit)  value:0x60E200
    SPI ADC Read  (24-bit)  value:0xE0E200
    SPI ADC Read Byte value:0xFE
    /*********************************No of Register Written Count: 184**********************************/
    SPI ADC Write (24-bit)  value:0x60F400
    SPI ADC Read  (24-bit)  value:0xE0F400
    SPI ADC Read Byte value:0xFE
    /*********************************No of Register Written Count: 185**********************************/
    SPI ADC Write (24-bit)  value:0x60F500
    SPI ADC Read  (24-bit)  value:0xE0F500
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 186**********************************/
    SPI ADC Write (24-bit)  value:0x60FB01
    SPI ADC Read  (24-bit)  value:0xE0FB01
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 187**********************************/
    SPI ADC Write (24-bit)  value:0x60FC01
    SPI ADC Read  (24-bit)  value:0xE0FC01
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 188**********************************/
    SPI ADC Write (24-bit)  value:0x400300
    SPI ADC Read  (24-bit)  value:0xC00300
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 189**********************************/
    SPI ADC Write (24-bit)  value:0x400420
    SPI ADC Read  (24-bit)  value:0xC00420
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 190**********************************/
    SPI ADC Write (24-bit)  value:0x4002F9
    SPI ADC Read  (24-bit)  value:0xC002F9
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 191**********************************/
    SPI ADC Write (24-bit)  value:0x6074F4
    SPI ADC Read  (24-bit)  value:0xE074F4
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 192**********************************/
    SPI ADC Write (24-bit)  value:0x607501
    SPI ADC Read  (24-bit)  value:0xE07501
    SPI ADC Read Byte value:0xF4
    /*********************************No of Register Written Count: 193**********************************/
    SPI ADC Write (24-bit)  value:0x6076EF
    SPI ADC Read  (24-bit)  value:0xE076EF
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 194**********************************/
    SPI ADC Write (24-bit)  value:0x60770C
    SPI ADC Read  (24-bit)  value:0xE0770C
    SPI ADC Read Byte value:0xEF
    /*********************************No of Register Written Count: 195**********************************/
    SPI ADC Write (24-bit)  value:0x60780A
    SPI ADC Read  (24-bit)  value:0xE0780A
    SPI ADC Read Byte value:0xC
    /*********************************No of Register Written Count: 196**********************************/
    SPI ADC Write (24-bit)  value:0x6079FE
    SPI ADC Read  (24-bit)  value:0xE079FE
    SPI ADC Read Byte value:0xA
    /*********************************No of Register Written Count: 197**********************************/
    SPI ADC Write (24-bit)  value:0x608BF4
    SPI ADC Read  (24-bit)  value:0xE08BF4
    SPI ADC Read Byte value:0xA
    /*********************************No of Register Written Count: 198**********************************/
    SPI ADC Write (24-bit)  value:0x608C01
    SPI ADC Read  (24-bit)  value:0xE08C01
    SPI ADC Read Byte value:0xA
    /*********************************No of Register Written Count: 199**********************************/
    SPI ADC Write (24-bit)  value:0x608DEE
    SPI ADC Read  (24-bit)  value:0xE08DEE
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 200**********************************/
    SPI ADC Write (24-bit)  value:0x608E0D
    SPI ADC Read  (24-bit)  value:0xE08E0D
    SPI ADC Read Byte value:0xEE
    /*********************************No of Register Written Count: 201**********************************/
    SPI ADC Write (24-bit)  value:0x608F0A
    SPI ADC Read  (24-bit)  value:0xE08F0A
    SPI ADC Read Byte value:0xD
    /*********************************No of Register Written Count: 202**********************************/
    SPI ADC Write (24-bit)  value:0x6090FE
    SPI ADC Read  (24-bit)  value:0xE090FE
    SPI ADC Read Byte value:0xA
    /*********************************No of Register Written Count: 203**********************************/
    SPI ADC Write (24-bit)  value:0x60A2F4
    SPI ADC Read  (24-bit)  value:0xE0A2F4
    SPI ADC Read Byte value:0xA
    /*********************************No of Register Written Count: 204**********************************/
    SPI ADC Write (24-bit)  value:0x60A301
    SPI ADC Read  (24-bit)  value:0xE0A301
    SPI ADC Read Byte value:0xA
    /*********************************No of Register Written Count: 205**********************************/
    SPI ADC Write (24-bit)  value:0x60A4EF
    SPI ADC Read  (24-bit)  value:0xE0A4EF
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 206**********************************/
    SPI ADC Write (24-bit)  value:0x60A50C
    SPI ADC Read  (24-bit)  value:0xE0A50C
    SPI ADC Read Byte value:0xEF
    /*********************************No of Register Written Count: 207**********************************/
    SPI ADC Write (24-bit)  value:0x60A60A
    SPI ADC Read  (24-bit)  value:0xE0A60A
    SPI ADC Read Byte value:0xC
    /*********************************No of Register Written Count: 208**********************************/
    SPI ADC Write (24-bit)  value:0x60A7FE
    SPI ADC Read  (24-bit)  value:0xE0A7FE
    SPI ADC Read Byte value:0xA
    /*********************************No of Register Written Count: 209**********************************/
    SPI ADC Write (24-bit)  value:0x60B9F4
    SPI ADC Read  (24-bit)  value:0xE0B9F4
    SPI ADC Read Byte value:0xFE
    /*********************************No of Register Written Count: 210**********************************/
    SPI ADC Write (24-bit)  value:0x60BA01
    SPI ADC Read  (24-bit)  value:0xE0BA01
    SPI ADC Read Byte value:0xF4
    /*********************************No of Register Written Count: 211**********************************/
    SPI ADC Write (24-bit)  value:0x60BBEF
    SPI ADC Read  (24-bit)  value:0xE0BBEF
    SPI ADC Read Byte value:0xF4
    /*********************************No of Register Written Count: 212**********************************/
    SPI ADC Write (24-bit)  value:0x60BC0D
    SPI ADC Read  (24-bit)  value:0xE0BC0D
    SPI ADC Read Byte value:0xF4
    /*********************************No of Register Written Count: 213**********************************/
    SPI ADC Write (24-bit)  value:0x60BD0A
    SPI ADC Read  (24-bit)  value:0xE0BD0A
    SPI ADC Read Byte value:0xD
    /*********************************No of Register Written Count: 214**********************************/
    SPI ADC Write (24-bit)  value:0x60BEFE
    SPI ADC Read  (24-bit)  value:0xE0BEFE
    SPI ADC Read Byte value:0xA
    /*********************************No of Register Written Count: 215**********************************/
    SPI ADC Write (24-bit)  value:0x60D0FF
    SPI ADC Read  (24-bit)  value:0xE0D0FF
    SPI ADC Read Byte value:0xFE
    /***********/*********************************No of Register Written Count: 246**********************************/
    SPI ADC Write (24-bit)  value:0x400468
    SPI ADC Read  (24-bit)  value:0xC00468
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 247**********************************/
    SPI ADC Write (24-bit)  value:0x606800
    SPI ADC Read  (24-bit)  value:0xE06800
    SPI ADC Read Byte value:0x1
    /*********************************No of Register Written Count: 248**********************************/
    SPI ADC Write (24-bit)  value:0x1100
    SPI ADC Read  (24-bit)  value:0x801100
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 249**********************************/
    SPI ADC Write (24-bit)  value:0x1204
    SPI ADC Read  (24-bit)  value:0x801204
    SPI ADC Read Byte value:0x4
    /*********************************No of Register Written Count: 250**********************************/
    SPI ADC Write (24-bit)  value:0x5C87
    SPI ADC Read  (24-bit)  value:0x805C87
    SPI ADC Read Byte value:0x87
    /*********************************No of Register Written Count: 251**********************************/
    SPI ADC Write (24-bit)  value:0x1200
    SPI ADC Read  (24-bit)  value:0x801200
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 252**********************************/
    SPI ADC Write (24-bit)  value:0x400200
    SPI ADC Read  (24-bit)  value:0xC00200
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 253**********************************/
    SPI ADC Write (24-bit)  value:0x400300
    SPI ADC Read  (24-bit)  value:0xC00300
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 254**********************************/
    SPI ADC Write (24-bit)  value:0x400469
    SPI ADC Read  (24-bit)  value:0xC00469
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 255**********************************/
    SPI ADC Write (24-bit)  value:0x600201
    SPI ADC Read  (24-bit)  value:0xE00201
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 256**********************************/
    SPI ADC Write (24-bit)  value:0x700201
    SPI ADC Read  (24-bit)  value:0xF00201
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 257**********************************/
    SPI ADC Write (24-bit)  value:0x603700
    SPI ADC Read  (24-bit)  value:0xE03700
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 258**********************************/
    SPI ADC Write (24-bit)  value:0x703700
    SPI ADC Read  (24-bit)  value:0xF03700
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 259**********************************/
    SPI ADC Write (24-bit)  value:0x60323C
    SPI ADC Read  (24-bit)  value:0xE0323C
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 260**********************************/
    SPI ADC Write (24-bit)  value:0x70323C
    SPI ADC Read  (24-bit)  value:0xF0323C
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 261**********************************/
    SPI ADC Write (24-bit)  value:0x60333C
    SPI ADC Read  (24-bit)  value:0xE0333C
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 262**********************************/
    SPI ADC Write (24-bit)  value:0x70333C
    SPI ADC Read  (24-bit)  value:0xF0333C
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 263**********************************/
    SPI ADC Write (24-bit)  value:0x60343C
    SPI ADC Read  (24-bit)  value:0xE0343C
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 264**********************************/
    SPI ADC Write (24-bit)  value:0x70343C
    SPI ADC Read  (24-bit)  value:0xF0343C
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 265**********************************/
    SPI ADC Write (24-bit)  value:0x60353C
    SPI ADC Read  (24-bit)  value:0xE0353C
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 266**********************************/
    SPI ADC Write (24-bit)  value:0x70353C
    SPI ADC Read  (24-bit)  value:0xF0353C
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 267**********************************/
    SPI ADC Write (24-bit)  value:0x600180
    SPI ADC Read  (24-bit)  value:0xE00180
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 268**********************************/
    SPI ADC Write (24-bit)  value:0x700180
    SPI ADC Read  (24-bit)  value:0xF00180
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 269**********************************/
    SPI ADC Write (24-bit)  value:0x60070F
    SPI ADC Read  (24-bit)  value:0xE0070F
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 270**********************************/
    SPI ADC Write (24-bit)  value:0x70070F
    SPI ADC Read  (24-bit)  value:0xF0070F
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 271**********************************/
    SPI ADC Write (24-bit)  value:0x1204
    SPI ADC Read  (24-bit)  value:0x801204
    SPI ADC Read Byte value:0x4
    /*********************************No of Register Written Count: 272**********************************/
    SPI ADC Write (24-bit)  value:0x5600
    SPI ADC Read  (24-bit)  value:0x805600
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 273**********************************/
    SPI ADC Write (24-bit)  value:0x5700
    SPI ADC Read  (24-bit)  value:0x805700
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 274**********************************/
    SPI ADC Write (24-bit)  value:0x2000
    SPI ADC Read  (24-bit)  value:0x802000
    SPI ADC Read Byte value:0x0
    /*********************************No of Register Written Count: 275**********************************/
    SPI ADC Write (24-bit)  value:0x2010
    SPI ADC Read  (24-bit)  value:0x802010
    SPI ADC Read Byte value:0x10

  • Hi Bala Krishna,

    Your colleague Ravindra has posted on e2e related to the same issue:

    https://e2e.ti.com/support/data-converters/f/73/t/959827

    Please try my suggestion on that thread. 

    Regards,

    Vijay

  • Hi Vijay,

    Can You please share the configuration for using single Channel (channel-A) and disabling  channel B, I feel the when we use two channels, the IC is being thermal shutdown and we are getting lane errors.

    Thanks & Regards

    Bala Krishna

  • Hi Bala Krishna,

    chB is enabled on reset ('PDN chB' register bit is 0 by default). So after reset when Powerup_Analog_Config is run, device goes to almost full current state. If board is not designed for this power consumption, device will go into shutdown. 

    To power down chB, set below two highlighted register bits to high:

    Regards,

    Vijay