Ii. Test conditions: Data sent
Static const unsigned char SineTable[101]=
{3,8,16,24,32,48,56,63,71,79,86,94,101, 109, 116, 123, 130, 137, 143, 150, 156, 163, 169, 175, 180, 186, 191, 196, 201, 206, 211, 215, 219, 223, 227, 231, 234, 237, 240, 243, 245,247, 249, 250, 252, 253, 254, 254, 254, 254, 254, 254, 253, 250, 249, 245, 243, 240, 237, 234, 231, 227, 223, 219, 215, 211, 206, 201, 196, 191, 186, 180, 175, 169, 163, 150, 143,137, 130, 123, 116, 109, 101, 94,86,79,71,63,56,48,40,32,24,16,8,0,};
Iii. Test results of 580KHz clock
Note: The yellow line is the waveform generated by TI's DAC chip TLC5602C and the blue line is the waveform generated by SC's DAC chip.Now our DAC chips have a lot of volatility when converted.
Iv. Test results when the clock is 137Hz