This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC43608: Output Fluctuaiton

Part Number: DAC43608

Hi there,

My customer is evaluating DAC43608. And he got a waveform like below.

The blue wave is 3.3V power supply, which is slightly fluctuating. VrefIN is connected to this power supply. 

The pink wave is 0V output. Why output is also fluctuating and has a phase shift between power supply? It should be straight as GND. Do we have any method to cancel the noise?

Also, he is using DEVICE_CONFIG register to turn off/on the output. Turn on output then modify output value, or modify output value then turn on the output, which is the better sequence?

Best,

Zeming