Currently, I would like to acquire digital data obtained by converting analog inputs from AIN0 to AIN3 with ADS1260 in order (at the same time as possible).
I have a question about the procedure and speed at that time.
About the procedure
The procedure is as follows, is it correct?
1. Wait for DRDY to go low
2. Enter High for START
3. Set MUXP to AIN0 and MUXN to AINCOM with WREG Command (AINCOM is connected to GND)
4. Wait for DRDY to go low and get the conversion data with RDATA Command
5. Set MUXP to AIN1 and do the same as 3 and 4.
6. Set MUXP to AIN2 and do the same as 3 and 4.
7. Set MUXP to AIN3 and do the same as 3 and 4.
About speed
How long does it take for each piece of data to be acquired while switching the target of the analog input for acquiring digital data as described above?
Is it 25us because it is 40kSPS? Or is the 179us described in the Conversion Latency of the data sheet the fastest?
Also, if there is a setting / procedure that can be acquired earlier than the above procedure, it would be helpful if you could let me know.
Thank you.