Other Parts Discussed in Thread: DAC7811
Hi,
I went through all the questions asked regarding DAC8811. But I still unable to understand.
I saw that serial interface maximum speed is 50Mhz. but the settling time is 0.5us which means 2Mhz.
I have the input which has the max sped of 2MSPS. As the settling time is also same.
I want to understand that, whether I can use the full code or not.
In datasheet there is a figure 9 which has some explanation, but I am unable to understand that.
I just want to understand that will this DAC work fine for 2MSPS speed?
Regards,
Rohit Arora