Hello
I have a customer who is looking to measure load cells with capacities up to 34 tons, with a maximum excitation of 15 V and sensitivity of 0.1 mv/V. They are interested in the ADS1232, however I wanted to ensure that device would work with an excitation voltage of 15 V. How does the excitation voltage correlate to which ADC to use for a weigh scale application?