Team,
I am still confused about the application of ADS1120, so I would like to list more questions:
1. What is the function AVDD and AVSS? Where do they connect to?
2. What is the function of VREF if choose internal VREF?
3. If AVDD is tied to 5V, AVSS is tied to GND, VREF is choosing internal Vref, and bi-directional current need to be measured, which means that the shunt voltage is from -5V to 5V, could ADS1120 sample this voltage directly using the differential input? If it can, what is the value that could be read after ADC?
Wish to get your reply, thanks!