Other Parts Discussed in Thread: DAC38J84
Hi
I'm trying to SYNC between FPGA and DAC37J84.
But SYNC signal doesn't become "H" and config 100 register ,shows alarm below.(other bit is '0')
bit10 = code synchronization error
bit9 = 8b/10b not-in-table code error
bit8 = 8b/10b disparity error
bit1 = read_error : Asserted if read request with empty FIFO
bit0 = read_empty : FIFO is empty
What do you think is wrong?
My DAC configration is below
LMF K = 244 16 interpolation =4 DAC data input Rate 153.6MSPS
INPUT DACCLOCK = 614.4MHz Serdes line rate 6.144Gbps
PLL_ENA=0,serdes refclksel =0, serdes_refclk_dev=1/2,MPY=0050,RATE=0128(HALF RANGE),JESDCLK_DIV=0x2000
CLK looks sine wave and lane eye pattern is open.
I added configuration below.Could you please check my configuration ,too?
0 0X0002 0X2072
0 0X001A 0X0025
0 0X0031 0X1000
0 0X0032 0X0000
0 0X0033 0X0100
0 0X003B 0X0800
0 0X003C 0X0050
0 0X003D 0X0088
0 0X003E 0X0128
0 0X003F 0X0000
0 0X0046 0X0044
0 0X0047 0X190A
0 0X0048 0X31C3
0 0X0049 0X0000
0 0X004A 0X031E
0 0X005F 0X0123
0 0X0060 0X4567
0 0X0025 0X2000
0 0X0024 0X0020
0 0X0000 0X321B
0 0X0003 0XA300
0 0X004B 0X0E03
0 0X004C 0X0F01
0 0X004D 0X0300
0 0X004E 0X0F2F
0 0X004F 0X1C61
0 0X0050 0X0000
0 0X0051 0X00FF
0 0X0052 0X00FF
0 0X0053 0X0000
0 0X0054 0X00FF
0 0X0055 0X00FF
0 0X005C 0X1111
0 0X0061 0X0211
0 0X0012 0X0000
0 0X0013 0X0000
0 0X0014 0X0000
0 0X0015 0X0000
0 0X0016 0X5000
0 0X0017 0X0000
0 0X0018 0X0000
0 0X0019 0X5000
0 0X002E 0XFFFF
0 0X0008 0X0000
0 0X0009 0X0000
0 0X000A 0X0000
0 0X000B 0X0000
0 0X000C 0X0400
0 0X000D 0X0400
0 0X000E 0X0400
0 0X000F 0X0400
0 0X0010 0X0000
0 0X0011 0X0000
0 0X0001 0X0003
0 0X006E 0X0000
0 0X006F 0X0000
0 0X0070 0X0000
0 0X0071 0X0000
0 0X0072 0X0000
0 0X0073 0X0000
0 0X0074 0X0000
0 0X0075 0X0000
0 0X0076 0X0000
0 0X0077 0X0000
0 0X0078 0X0000
0 0X0079 0X0000
0 0X007A 0X0000
0 0X007B 0X0000
0 0X007C 0X0000
0 0X007D 0X0000
0 0X0022 0X1B1B
0 0X0023 0X01FF
0 0X0026 0X0000
0 0X002D 0X0001
0 0X0004 0XFCFC
0 0X0005 0X0000
0 0X0006 0XFFFF
0 0X0057 0X00FF
0 0X0058 0X00FF
0 0X005A 0X00FF
0 0X005B 0X00FF
0 0X0064 0X0000
0 0X0065 0X0000
0 0X0066 0X0000
0 0X0067 0X0000
0 0X0068 0X0000
0 0X0069 0X0000
0 0X006A 0X0000
0 0X006B 0X0000
0 0X006C 0X0000
0 0X006D 0X00F0
0 0X001E 0X3333
0 0X001F 0X3320
0 0X001F 0X8880
0 0X001F 0X8882