This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC084S085: Edge rate or rise/fall time requirement

Part Number: DAC084S085

Hi,

Good day.

Our customer would like to know if DAC084S085 has an edge rate or rise/fall time requirement for the SCLK pin. The datasheet does not call out a rise/fall time specification, and they want to know if the SCLK input signal must meet a certain rise/fall time or edge rate to work properly.

Thank you for your support.


Regards,

Cedrick

  • Hi Cedrick,

    If there is no rise/fall time specified in the datasheet, then the only requirements that the SCLK will have to meet are the timing requirements given in table 7.6 of the datasheet. The SCLK pulse needs to be high for at least 10ns, and low for at least 10ns. The datasheet gives the input high voltage as at least 2.4V and an input low voltage of below 0.8V for a supply of 5V.

    We recommend not exceeding a rise/fall time of 500ns to avoid extra current being consumed by the device.