Other Parts Discussed in Thread: ADS4229, LP5910
Dear Sir,
We have an application where we are using the DAC3171 14-bit D/A convertor.
We have it working on our board, clocked with a 500 Mhz clock, steered by a Xilinx arxiv FPGA, rendering a 171 Mhz data signal at full scale.
Now, it is working correctly, with great performance. Only, we see AM modulation on the signal @-60 db relative to the carrier.
The AM modulation frequency is about 100 kHz, and this is the resonance frequency of the L-C circuits used for the power supply decoupling.
The DAC has 4 supplies {Vcc1V8_DAC_CLK, Vcc1V8_DAC, Vcc1V8_DAC_IOVDD, Vcc1V8_DAC_DIG} decoupled with a
Murata Ferrite bead BLM15EX471SN1D and a ceramic capacitor of 1 uF (+ an additional 1 nF). These circuits have a resonant
frequency around 100 Khz and we see the DAC amplitude modulate the output (-60 dB down) at 100 Khz.
The 3.3 Volt supply is direct from a regulator.
Note that we found this issue elsewhere on the board too. The 500 Mhz clock is produced by a 250 Mhz doubler, and likely has
some amplitude modulation, but no more than -50 dB.
Q.
- Are you sure this LC power supply decoupling is OK ?. We have a suspicion this problem is caused by the supply/DAC
combination.
- Would it be better to eliminate the ferrite beads and just use LDO regulators ?. (The board is full of LDO's anyway.)
- Are there some supplies more sensitive than others ?.
Q.
- Note: We have the ADS4229 on the same board, decoupled in the same way. Does it also have this sensitivity ?.
(I cannot measure).