This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM98640QML-SP: voltage divider at input and current leakage impact

Part Number: LM98640QML-SP

Hello,

In one of our camera application, we would like to use the LM98640. The output sensor voltage is single-ended and supplied with +5V. Therefore, we need to implement a voltage divider with two 100Ohm resistors covered by an amplifier between the sensor and the AFE  (see diagram). We are wondering if there would be a problem to connect the AFE input to the divider considering the sample and hold input leakage of the AFE ? Is this current leakage happening during the sample phase ?

Kind regards,

Thibaut