Other Parts Discussed in Thread: AMC1306M25, AMC1336
I am looking to sense the voltage across a MOSFET in a flyback power converter. I start by stepping the voltage down to about 3V.
Since my input voltage is 300V, I need to then isolate this signal such that I can pass the information to my DSP from TI and measure the voltage across the FET safely. The switching frequency is 1MHZ, so I believe an analogue Linear isolator With 300kHz-400kHz bandwidth will not be sufficient in achieving the response speed that I need to fully reflect the high frequency voltage signals.
I came across this device which is an isolated modulator which has a high clock speed.
Since digital signals can have theoretically unlimited bandwidth, would these devices work well in replicating a 1MHZ analogue signal with fast response time, rise and fall time?
The voltage that I will measure will not be a differential voltage. The data sheet mentions that the maximum differential voltage is in the mV range. If we tie the negative analogue input to ground and simply pass a 3V analogue signal to the positive analogue input, will the device still work as intended and replicate a 3V output at the digital side which accurately reflect a 3V analog at the input side? The data sheet does mention that the max analogue input is equal to the 5V supply rail of the high voltage side, but the application examples only really use it for differential current sensing - I want to use it for ground referenced voltage sensing.
Thanks in advance!