Hello, I would like to ask about the potential failure mechanism in the LMP92066 during 125°C operation or also in the event the temperature of 125°C is exceeded (estimate of 135°C)
Would this device have graceful degradation, like a shift in the analog voltage at the DAC output or could it have a hard failure like a thermal shutdown if for example the device exceeds the 125°C.
My prior question on this device was about data retention over ten years, and the answer was that the device was baked at high temperatures. Was that high temperature bake applied during operation?