Hi,
following changes were made to EVM board :
• Remove C2 and C3, populate R171 and R174
• Remove C60 and C61, populate C52 and C306
• Uninstall Jumper J13
after that TSW and EVM were connected, Fs selected is 1600 MHz . TSW Fs is set to 3200 MHz.
JMODE1 is selected on both the GUIs.
SYNC led D3 is still high, and refclk LED doesn't blink.
is there any configuration that is missing.
thanks.
Anjana