Other Parts Discussed in Thread: ADS1260
Hi team
What is the recommended reference voltage of ADS1251?
I mean, it seems that 4.096V is recommended as the reference voltage. So if the reference voltage is 1.5V or 2.5V, are there any differences compared to Vref=4.096V?
Could you also tell the best device that can meet requirements as below, if the device is better than ADS1251?
Resolution: 24bit
Conversion Rate: more than 20kHz
input type: differential
# of ch: 1
Regards,
Noriyuki Takahashi