Hi expert,
Please share some comments for below customer questions.
1. if under mode continuous-conversion IC is not entering power-down mode, is that correct?
2. If we set Mode into continuous-conversion, and re-write value to MUX[2:0], then waiting for how long to read back the value, would be the good time to read back conversion result for the new MUX setting?
3. If customer require to read value from Ch1~ CH4, is the mode suggested to be set into continuous -conversion?
4. If the application is single ADS1015, Can we keep Config Register[4:0] as default?