Hi,
- What is the filter order and characteristics of LNA HPF?
- What is the filter order and characteristics of PGA HPF?
- It is mentioned in datasheet that PGA LPF is a third order filter with Butterworth characteristics and a typical 18-dB per octave roll-off. Suppose I am running the ADC(in 14 bit) at 20 MHz and LPF cut-off is at 10 MHz. Will it act as an anti-aliasing filter? The attenuation at 20 MHz will only be 36-dB. As per my understanding a 14-bit ADC needs at least 84 dB attenuation before Fs/2 (here 20/2 = 10 MHz). Correct me if I am wrong. Do I need to use any external filters?
- I am using this AFE58JD18 for sonar application. It has two frequencies of operation: 1: 105kHz with 20 kHz Bandwidth and 2: 500kHz with 50kHz bandwidth. The input signal to AFE ranges from 215 nVpp to 4 mVpp approx. Do I need to use external pre amplifier for amplifying this signal or AFE58JD18 is sufficient?
- I am planning to implement Digital TGC. I will adjust the VCAT attenuation from 42dB to 0 dB in 6-dB steps for each scan through SPI. Correct me if I am wrong. What to do with AFE TGC pins if I am implementing Digital TGC.
- Is there any document mentioning how to calculate noise level introduced by AFE?
Thanks,
Nidhal