This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC04: TLC04 FILTER CUT OFF FREQUENCY ISSUES

Part Number: TLC04


hi,

  i am using this filter in my design. i need cut off frequency of 200Hz,so i have set C=0.1uF and R=560 ohms( i have changed on board which  is not same as in schematic) for which clock frequency will be 10.5KHz (not an issue).

I have fed a sine wave but i could see the peak to peak voltage drop after 20Hz only is this correct? .i am not able to understand what is the issue.i think these Capacitor and resistor values are good enough for 200Hz cut off frequency. where i am doing mistake ? please reply asap. i have attached the schematic.