This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC71416: is connected to FPGA, and we are using 50 MHz as SCLK, but DAC is not configuring

Part Number: DAC71416

DAC 71416 is connected to FPGA, using 50 MHz as SCLK, but DAC is not configuring, the supply voltage given to VIO is 3.3 V,

and we are matching the timing requirement also but it is not getting configured. But it is configured with SCLK of frequency 25MHz.

Thanks in advance.