Hi Team,
Our customer is currently considering DAC81404 as a candidate for a new product. He has reviewed the datasheet and some of the applications which shows that it is primarily a high current, remote power supply controller utilizing the sense lines. However, his application is different from the references provided and would like to know what to do with the sense lines if they are not used. How should the sense lines be treated? In his application, the DAC output would provide voltage to a load but the return current does not have a dedicated line, it merely follows the common ground plane. The current in the load is only 10 mA so it would seem IR drops are low and the sense line feedback and compensation is not necessary. He doesn't have spare connector pins for sense lines to the remote load.
Regards,
Danilo