Hi,
I would like to confirm the circuit that we designed to interface with 3 kind of RTD (PT50, PT100 and PT500). All probes are 3-wires.
Attached is the circuit that we have with the ADS1248IPWR.
We are using the TMS5703137DPGEQQ1 as a microprocessor.
We are using 2 ADC, each ADC interfaces with one 3-wires RTD and other analog inputs. The attached circuit only shows one of the ADC but the second is the exact same circuit.
Communication work well but I have some concerns about the circuit and the readings on the 3-wire RTD.
As you can see below, we are doing 2 reading: 1st between Hi and Sense and 2nd between Sense and Lo.
Can you confirm that we need to subtract the second reading from the first reading to remove the lead effect?
Also, I think we need to remove the 100 Ohm resistor from the second reading as we are currently reading about 100 Ohm.
Or do we need to remove the 100 Ohm resistor from the circuit?
Can you confirm that I don’t need capacitor between ANI1 and ANI2 when I read the Sense to Lo?
Register Name | Bit | Setting | Description | |
Common: Initial device setup | ||||
IDAC0 | DRDY MODE | 0 | DOUT/_DRDY pin functions only as Data Out | |
IMAG | 110 | Excitation current = 1mA | ||
IDAC1 | I1DIR | 10x0 | IEXC1 (x=don't care) | |
I2DIR | 11xx | Disconnected (x=don't care) | ||
Common: Reset PGA to 1 | ||||
SYS0 | PGA | 000 | Gain=1 | |
DR | 0111 | 640 SPS | ||
TAT/ADPT setup | ||||
MUX1 | VREFCON | 01 | Internal reference always On | |
REFSELT | 00 | REFP0/REFN0 selected | ||
MUXCAL | 000 | Normal operation | ||
SYS0 | PGA | 000 | Gain=default to 1, depends on installed probe | |
DR | 0111 | 640 SPS | ||
Channel: TAT_HI/ADPT_HI | ||||
MUX0 | BCS | 00 | Burn-out current source Off | |
MUX_SP | 000 | AIN0 | HI | |
MUX_SN | 001 | AIN1 | SENSE | |
Channel: TAT/ADPT SENSE | ||||
MUX0 | BCS | 00 | Burn-out current source Off | |
MUX_SP | 001 | AIN1 | SENSE | |
MUX_SN | 010 | AIN2 | LO | |
AOA/AOS/DIODE/BITE set reference | ||||
MUX1 | VREFCON | 01 | Internal reference always On | |
REFSELT | 01 | REFP1/REFN1 selected | ||
MUXCAL | 000 | Normal operation | ||
AOA/AOS configuration | ||||
SYS0 | PGA | 000 | Gain=1 (same for all probe) | |
DR | 0111 | 640 SPS | ||
Channel AOA/AOS Hi | ||||
MUX0 | BCS | 00 | Burn-out current source Off | |
MUX_SP | 011 | AIN3 | HI | |
MUX_SN | 111 | AIN7 | LO | |
Channel AOA/AOS Wiper | ||||
MUX0 | BCS | 00 | Burn-out current source Off | |
MUX_SP | 100 | AIN4 | WIPER | |
MUX_SN | 111 | AIN7 | LO | |
Channel: DIODE PS/DIODE PT | ||||
MUX0 | BCS | 00 | Burn-out current source Off | |
MUX_SP | 101 | AIN5 | ||
MUX_SN | 111 | AIN7 | ||
SYS0 | PGA | 001 | Gain=2 (same for both diodes) | |
DR | 0111 | 640 SPS | ||
Channel: BITE | ||||
MUX0 | BCS | 00 | Burn-out current source Off | |
MUX_SP | 110 | AIN6 | ||
MUX_SN | 111 | AIN7 | ||
SYS0 | PGA | 000 | Gain=1 | |
DR | 0111 | 640 SPS |
Best,
Sabine Pennavayre-Guirand