Part Number: ADC128S052
I adopted your ADC128S052CIMTX / NOPB, but when I checked the AD value that was taken in, it was found that the fluctuation was large (about ± 3%).
After checking the situation, the data sheet of ADC128S052CIMTX / NOPB recommends 1uF + 0.1uF as the input capacitor, so it was mounted as an input capacitor, but the reference power supply adopted depends on this load capacity , It was oscillating.
It is best to change the reference power supply, but since we have already manufactured the board, we are considering whether it can be supported by changing the constant.
As a test, when I removed the capacitor, the oscillation stopped, but noise occurred at the timing of AD conversion.
Therefore, when only 0.1uF was used, there was no oscillation or noise, and there was no fluctuation in the AD value.
Also, when 0.1uF was changed to 0.01uF, noise such as spike noise occurred, but the AD value did not fluctuate.
Even if the input capacitor is made smaller, it seems that the AD value is not affected. Is there any problem?
Thank you for your reply.