Dear TI experts:
AFE5812 is designed for ultrasonic applications, while my application is a 8-channel radar receiver. I want to interface 8 differential opamps to the inputs of AFE5812, but it seems that the INM pins are designed to connect Cbypass to ground, only the INP pins are used.
Can I directly connect the input Vin+ to INP and Vin- to INM?
Thanks,
Jhon