Dear TI expert,
I am reading SLWU087D, in the Introduction, I quote "provide high speed data transfers (2Gbps USB 3.0
systems, 320Mbps USB 2.0 systems) between the host pc and the pcb.".
Should it be 5 Gbps if it is compliant with the USB 3.0 standard?
"With a 3.0 system, the user can capture 1GBytes in ≈ 20 seconds. With a 2.0 system, around 45 seconds."
Even use the 2.0Gbps, the time difference should be about 1 to 6 ratio. which is around 7 seconds.
Did I miss anything here?
Thanks,
David