Other Parts Discussed in Thread: AMC7836
I'm trying to read/write from the AMC7836 registers. I'm using the SDM-USB-DIG platform and TI's WIN 7 GUI Software. The VDUT is 3.3V but the SPI signals are only 1.8Vp-p. The AMC7836 requires 0.7 * IOVDD ( 0.7 * 3.3) which is 2.31V min for a min logic high. The Microcontroller (MPS430) on the SDM-USB-DIG states that at VCC = 3V the High Level Output (Voh) = VCC - 0.6V or 2.7V(min). The voltage level translator between the MCU and the AMC7836 has +3.3V for both VCCA and VCCB. So I can see no way that the SPI SCLK, SDI, CS signals can only be 1.78V p-p. Also SDO which originates at AMC7836 also only 1.8V p-p signal level. How can this be? What I'm missing here?