Other Parts Discussed in Thread: THS4521
Hi,
We have a problem when using ADS8885 with THS4521 as ADC buffer.
When VINN/VINP input near to 4V and Vref=4.096V, there would be around +/-1000 value variation at the digital output.
This problem would be solved when the input be smaller like 3V or less. (only +/-7 value variation at the digital output.)
The problem also be found when input=5V and Vref=5V.
The power for THS4521 is always 5V.
My questions are what may cause this problem and how could we solve it?
Thank you.
Best Regards,
Cindy